EIP.PACKETMISSTHRESHOLD
Description
This parameter defines the threshold of the counter used to trigger F7005 Cyclic Setpoints Missing for EtherNet/IP. The missed packet counter (EIP.MISSEDPACKETCOUNT) increments by 3 on every missed cyclic packet and decrements by 1 when a packet is received. By default, the threshold is set to 9. If the threshold is set to 0, the fault is disabled.
Examples
The following chart provides an example of how the fault counter behaves using the default threshold of 9:
|
Fieldbus Cycle |
Packet Received |
Counter |
Faulted |
|---|---|---|---|
|
0 |
Yes |
0 |
No |
|
1 |
Yes |
0 |
No |
|
2 |
No |
3 |
No |
|
3 |
Yes |
2 |
No |
|
4 |
Yes |
1 |
No |
|
5 |
No |
4 |
No |
|
6 |
No |
7 |
No |
|
7 |
Yes |
6 |
No |
|
8 |
No |
9 |
Yes |
|
9 |
Yes |
8 |
Yes |
|
10 |
Yes |
7 |
Yes |
|
11 |
Yes |
6 |
Yes |
Context
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-10-04-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 (disabled) to 216 |
|
Default Value |
9 |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
EtherNet/IP drives: AKD2G-SPI
Industrial Ethernet Information
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
3902 |
1 |
3902 (0xf3e) |
EIP.PACKETMISSTHRESHOLD |
Unsigned16 |
Read/Write |
Yes |